Indoor location system for the distribution warehouse - LPS solution powered by Locix

3:03

This is an introduction of LPS (local positioning system) solution, which can locate the position of tags attached to humans or things with the multiple fixed stations (Anchor) installed in the distribution warehouse. With precise sub 1m positioning, LPS can be used for the purposes such as improving the worker's flow-line and the productivity in the warehouse. The positioning is calculated in real time in the cloud using Locix's proprietary algorithms and provides the location data via API.

View More
View Less

Share this video

Embed