Pulse Signal Unit <Wireless Sensing Solution>
1:58
Here is a pulse signal unit that can be installed on existing sensors to automate data collection. The accumulated data can also be analyzed to determine the cause and the extent of the impact of any problems.
Related Videos
For "wireless"
-
Play video Low Frequency (LF) Wireless Communication Using Murata's LF Antennas: Stable and Highly Accurate Distance Measurement and Position Detection Using Magnetic Fields (Magnetic Field Ranging & Positioning)
Low Frequency (LF) Wireless Communication Using Murata's LF Antennas: Stable and Highly Accurate Distance Measurement and Position Detection Using Magnetic Fields (Magnetic Field Ranging & Positioning)
Here, we explain about the basic principles and features of wireless communication using magnetic fields for low frequency (LF) wireless communication using Murata's LF antennas. We take a look at the benefits of this technology, such as offering sta
2:40
-
Play video Traffic counter system
Traffic counter system
The video introduces the traffic counter system using wireless sensor mesh network. Show more
2:01
-
Play video Basic Knowledge of Wireless Communication: Wireless Mechanism Part 2
Basic Knowledge of Wireless Communication: Wireless Mechanism Part 2
This video looks at the direction in which data travels (transmission modes). This is one of the important specifications of wireless devices and is rarely comprehensively explained. We explain in this video that there are two transmission modes:
3:21
-
Play video Vibration Sensor Unit <Wireless Sensing Solution>
Vibration Sensor Unit
Here is a wireless vibration sensor unit that achieves a wide range of measurement frequencies and long battery life for its vibration sensor unit by making use of the company’s knowledge of piezo-ceramic elements that was cultivated over Show more..
2:33
-
Play video Basic Knowledge of Wireless Communication : What Is a Communication Protocol?
Basic Knowledge of Wireless Communication : What Is a Communication Protocol?
In this video, we will take a look at communication protocols. Communication protocols are the common rules necessary to reliably exchange data between different devices and networks.
6:29
-
Play video Basic Knowledge of Wireless Communication: Wireless Mechanism Part 1
Basic Knowledge of Wireless Communication: Wireless Mechanism Part 1
This video looks at the basic matters regarding wireless communication. This includes what wireless communication is, the different types, application examples, and its core modulation technology.
5:00