Improving Factory Access Control and Evacuation Management | Implementation Manager Discusses LF Antenna Application Case Study [Okayama Murata Manufacturing]
2:39
Factory access control and evacuation verification require systems that are capable of accurately tracking the situation without impeding the flow of people. Murata’s LF antennas determine the direction of human movement with a direction detection technology based on LF communication that achieves smooth access control. They prevent the disruption of traffic flows even during crowded periods and can be utilized to track the evacuation status and presence of people during emergencies. This video presents an interview with the manager regarding the implementation effectiveness and on-site changes based on an implementation case study conducted at Okayama Murata Manufacturing. ▼Recommended for the following viewers: ・Persons looking to review access control at factories ・Persons evaluating the streamlining of evacuation verification and safety confirmation ・Persons interested in learning about actual implementation case studies and user feedback