Video Player is loading.
Current Time 0:00
Duration 5:02
Loaded: 0.00%
Stream Type LIVE
Remaining Time 5:02
 
1x
  • Chapters
  • descriptions off, selected
    • captions off, selected
    • en (Main), selected

    No.2 "The Measurement process for the oscillation margin" - IC and crystal units characterization -

    5:02

    18 Aug. 2020

    What is the Oscillation margin? Oscillation margin provides the limit at which oscillation stops. This is one of the most important parameters for the oscillation circuit. We would like to explain the measurement process to acquire the oscillation margin.

    View More
    View Less

    Share this video

    Embed