Drone control and automated landing using LF communication
1:27
Murata LF antennas can be used for accurate position measurement. By using a drone in combination with LF antennas, it is possible to implement drone control and automated landing. Let’s see how it works.
Related Videos
In All Videos
-
Play video Demo of position detection using LF communication
Demo of position detection using LF communication
Murata LF antennas can be used for accurate distance measurement. By using three LF transmitter antennas in combination, it is possible to achieve more accurate position detection than that with existing methods employing radio waves. Let’s see how i
1:34
-
Play video LF communication is robust despite obstacles such as metal objects and the human body.
LF communication is robust despite obstacles such as metal objects and the human body.
As LF communication signals can pass around and through obstacles, reception is not affected by obstacles such as metal objects and the human body. Let’s see how it works.
2:00
-
Play video Advancing Healthcare with Sensor Components for Implantable Devices
Advancing Healthcare with Sensor Components for Implantable Devices
Murata's technologies are continuously becoming smaller and smarter, driving the advancement of medical implantable devices.
5:41
-
Play video “Vision 2030: What Murata Manufacturing Wants to Be” in 90 Seconds
“Vision 2030: What Murata Manufacturing Wants to Be” in 90 Seconds
We support affluent lifestyles with electronic components that are essential for social infrastructure, and harness innovation to solve social issues and practice sustainable operations. Vision 2030, which outlines what Murata wants to be, is a visio
1:38
-
Play video Direction-independent LF communication using a triaxial LF antenna
Direction-independent LF communication using a triaxial LF antenna
Using a Murata triaxial LF receiver antenna enables reception of signals from any direction, X, Y, or Z. This video shows how reception is possible without the direction having any effect. Devices using LF antennas can be placed in a bag, for instanc
1:43
-
Play video Optimization of Medical Device Logistics Management Operations with id-Bridge™ Standard
Optimization of Medical Device Logistics Management Operations with id-Bridge™ Standard
You can see here the situations for which id-Bridge™ Standard has been used to optimize operations such as by reducing the burden of inspection work and speeding up stocktaking during the distribution of medical devices.
5:14