AMR Sensor (Magnetic Sensor) working principle
1:22
This video explains the resistance change when magnetic element detects the magnetic field.
Related Videos
In AMR Sensors (Magnetic Sensors)
-
Play video Murata's AMR Sensors: Opening/Closing Detection and Demos This video takes a look at ON/OFF detection with AMR sensors using the example of detecting the opening and closing of laptops and other devices.
Murata's AMR Sensors: Opening/Closing Detection and Demos This video takes a look at ON/OFF detection with AMR sensors using the example of detecting the opening and closing of laptops and other devices.
Contents presented in this video: ・ON/OFF detection of the open/closed state of laptops and other devices ・Adjustment of the detection position by changing the direction or placement of the magnets ・Detection near the hinge axis ...
3:12
-
Play video AMR Sensor Demo Video
AMR Sensor Demo Video
You can watch a demo using a sensor that can detect 1-axis and 3D (omnidirectional).
0:34
-
Play video AMR Sensor (Magnetic Sensor) for Pneumatic Cylinder
AMR Sensor (Magnetic Sensor) for Pneumatic Cylinder
This video explains the usage of AMR Sensor (Magnetic Sensor) in the cylinder. See the usage of position detection and the output signal of AMR sensor (Magnetic Sensor) .
1:07
-
Play video Explanation of how to use the AMR sensor simulation tool
Explanation of how to use the AMR sensor simulation tool
This video compares how the sensor turns on and off when a magnet actually approaches the sensor for each of the cases of opening/closing, sliding, and rotation, and how the magnet enters the detection area on the simulation tool.
2:33
-
Play video AMR Sensor (Magnetic Sensor) for Flow Meter
AMR Sensor (Magnetic Sensor) for Flow Meter
This video explains the usage of AMR Sensor (Magnetic Sensor) in various types of meter such as water meter and gas meter.See the usage of flow rate detection and the output signal of AMR sensor (Magnetic Sensor) .
2:31
-
Play video Murata's AMR Sensors: Rotation Detection and Demo This video takes a look at the application of AMR sensors using the example of rotation position detection for smart locks and other devices.
Murata's AMR Sensors: Rotation Detection and Demo This video takes a look at the application of AMR sensors using the example of rotation position detection for smart locks and other devices.
Contents presented in this video: ・Rotation position detection for smart locks and other devices ・ON/OFF detection of motor stopping positions ・Adjustment of the detection angle range by changing the direction and placement of the magnets ...
2:47