- 2x
- 1.75x
- 1.5x
- 1.25x
- 1x, selected
- 0.75x
- 0.5x
- Chapters
- descriptions off, selected
- captions settings, opens captions settings dialog
- captions off, selected
- en (Main), selected
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Low-noise: Operating noise
1:01
24 Apr. 2024
One feature of the microblower is its low-noise operation. In this demonstration, a microphone is used to capture the sound of the MZB3004T04's operation.
RELATED VIDEOS
-
動画を再生 High-speed airflow: Visualizing the flow of air
24 Apr. 2024
High-speed airflow: Visualizing the flow of air
The microblower is an unprecedented product that converts the vibrations of a piezoelectric material into an outrush of air. This demonstration visualizes the rapid flow of air from the nozzle.
0:37
-
動画を再生 Lightweight, high airflow rate: Hovering use
24 Apr. 2024
Lightweight, high airflow rate: Hovering use
The microblower is lightweight but can produce a high airflow volume. By making use of this feature, it is possible to cause an object to float on air like a hovercraft.
0:50
-
動画を再生 Thin and vibration-free: Aeration
24 Apr. 2024
Thin and vibration-free: Aeration
The features of the microblower include thinness and vibration-free operation. In this demonstration, microblowers are used as an air pump in a small water tank.
0:40
-
動画を再生 Negative pressure: Suctioning a viscous liquid
24 Apr. 2024
Negative pressure: Suctioning a viscous liquid
In this demonstration, a viscous liquid is suctioned. Note that the microblower is poweful enough to suction the viscous liquid.
0:45
-
動画を再生 Negative pressure: Crushing a plastic bottle (with suction)
24 Apr. 2024
Negative pressure: Crushing a plastic bottle (with suction)
The high pressure and high airflow volume generated by the MZB4001T05 can be used to produce suction. Here we will show how this high negative pressure can quickly crush an empty plastic bottle.
0:43
-
動画を再生 High pressure: Water fountain
24 Apr. 2024
High pressure: Water fountain
The pressurized air in the tank flows out suddenly, pressing on the liquid and propelling a jet of water from the nozzle. In this video, the water jet will reach a height of around 3 meters.
0:53