-
PTC Thermistor (POSISTOR) PRG series Application Example Resettable Fuses
This video takes a look at an example of overcurrent protection using the PRG series of PTC thermistors as a resettable fuse. The PRG series has the following features:
3:52
-
Mobility Market Applications (NTC and PTC Thermistors)
Thermistors provides temperature detection and current suppression to improve the performance and safety of equipment for electrification and automation.
3:48
-
Personal Electronics Market Applications (NTC and PTC Thermistors)
Mobile devices and wearable devices been improved on a daily basis to ensure that they are safe so that they can be worn and to make them smaller and lighter so that they can be carried. Thermistors play an active role in these devices.
2:39
-
FA Market Applications (NTC and PTC Thermistors)
Thermistors are used for temperature detection and current suppression to realize maintenance-free FA equipment to improve productivity, and achieve full automation.
2:49
-
How to choose a thermistor (NTC thermistor)
NTC thermistors have temperature sensing (for prevention or control) and temperature compensation (correction) features. This video explains the type of NTC thermistor to choose for each feature.
4:26
-
How to choose a thermistor (PTC thermistor)
PTC thermistors have temperature sensing (for prevention) and current control (protection) features. This video explains the type of PTC thermistor to choose for each feature.
3:12
-
Overheat Sensing at Multiple Locations
It's linked and more than one points of abnormal overheating is detected in series !
10:24
-
LED Overheat Protection
A set and a part are protected from abnormal fever, overheating by differential temperature in the temperature rise test, plunge electric current and over-current!
5:08
-
Chip PTC Thermistors (POSISTOR™) for Wireless Power Transfer System
We introduce Chip PTC Thermistor corresponding to wireless electricity supply (POSISTOR™). Show more
1:38