Under Development – Demo of Static Electricity Elimination Using the IonissimoTM MHM330 Type Ionizer Module: Comparison of the State of Coffee Powder Adhesion in a Coffee Mill

1:56

The IonissimoTM MHM330 type is equipped with our unique technology that makes it possible to adjust the amount of positive and negative ions generated to realize highly accurate static electricity elimination. This video presents a demo of the elimination of the static electricity generated in a coffee mill. You can confirm that the coffee powder adheres to the coffee mill or flies around due to the static electricity generated when milling the coffee beans before use of the MHM330 type. You can then see that the static electricity is effectively eliminated and that coffee powder adhesion to the coffee mill or flying around is suppressed after use of the MHM330 type.

View More
View Less

Share this video

Embed