- 2x
- 1.75x
- 1.5x
- 1.25x
- 1x, selected
- 0.75x
- 0.5x
- Chapters
- descriptions off, selected
- captions settings, opens captions settings dialog
- captions off, selected
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Chip PTC Thermistors (POSISTOR™) for Wireless Power Transfer System
1:38
04 Sep. 2014
We introduce Chip PTC Thermistor corresponding to wireless electricity supply (POSISTOR™). When using POSISTOR™, abnormal fever of a metallic thing by the electromagnetic field which occurs at the time of non-contact electricity supply of an EV and PHEV is detected.
RELATED VIDEOS
-
動画を再生 LED Overheat Protection
04 Sep. 2014
LED Overheat Protection
A set and a part are protected from abnormal fever, overheating by differential temperature in the temperature rise test, plunge electric current and over-current!
5:08
-
動画を再生 Overheat Sensing at Multiple Locations
04 Sep. 2014
Overheat Sensing at Multiple Locations
It's linked and more than one points of abnormal overheating is detected in series !
10:24
-
動画を再生 How to choose a thermistor (PTC thermistor)
14 Jun. 2023
How to choose a thermistor (PTC thermistor)
PTC thermistors have temperature sensing (for prevention) and current control (protection) features. This video explains the type of PTC thermistor to choose for each feature.
3:12
-
動画を再生 How to choose a thermistor (NTC thermistor)
14 Jun. 2023
How to choose a thermistor (NTC thermistor)
NTC thermistors have temperature sensing (for prevention or control) and temperature compensation (correction) features. This video explains the type of NTC thermistor to choose for each feature.
4:26
-
動画を再生 FA Market Applications (NTC and PTC Thermistors)
05 Dec. 2023
FA Market Applications (NTC and PTC Thermistors)
Thermistors are used for temperature detection and current suppression to realize maintenance-free FA equipment to improve productivity, and achieve full automation.
2:49
-
動画を再生 Personal Electronics Market Applications (NTC and PTC Thermistors)
14 Dec. 2023
Personal Electronics Market Applications (NTC and PTC Thermistors)
Mobile devices and wearable devices been improved on a daily basis to ensure that they are safe so that they can be worn and to make them smaller and lighter so that they can be carried. Thermistors play an active role in these devices.
2:39