-
Vibration Sensor Unit Assembly Procedure
This video explains the assembly procedure for the Vibration Sensor Unit and important precautions to follow during assembly.
1:52
-
Integrated Renewable Energy Control Solution efinnos Overview
Must See: New Standard for Decarbonization and Cutting Electricity Bills! In this video, we introduce the benefits of effinos, which is used in Murata Manufacturing's plants in Japan.
1:49
-
Integrated Renewable Energy Control Solution efinnos Implementation Example
Must See: New Standard for Decarbonization and Cutting Electricity Bills! We look into the secrets of Kanazu Murata Manufacturing, which has been featured in many media outlets in Japan.
2:25
-
Wi-Fi® sensing for child presence detection Demonstration
This is a demonstration of detecting an infant left in a vehicle.
1:17
-
Wi-Fi® sensing for child presence detection Overview
The Wi-Fi® sensing solution features 1: easy installation, 2: flexibility of installation location, and 3: a wide detection area, contributing to the new standard for NCAP compliance.
1:23
-
Vibration Sensor Unit
Here is a wireless vibration sensor unit that achieves a wide range of measurement frequencies and long battery life for its vibration sensor unit by making use of the company’s knowledge of piezo-ceramic elements that was cultivated over Show more..
2:33
-
Temperature Humidity Sensor Unit
Here is a wireless temperature and humidity sensor unit that can be easily installed and expanded. Show more...
2:55
-
Pulse Signal Unit
Here is a pulse signal unit that can be installed on existing sensors to automate data collection. The accumulated data can also be analyzed to determine the cause and the extent of the impact of any problems.
1:58
-
CT Sensor Unit
Here is a wireless CT sensor unit that can be installed on equipment powered by a single-phase AC or three-phase AC power supply, such as three-phase heaters and motors that are essential to the infrastructure of buildings and factories, Show more..
2:06
-
Wireless Sensor network solution for factories and buildings
Murata's Wireless Sensing Solution will enable you perform remote monitoring. Collected data can be used for the maintenance and efficiency improvement of factories and buildings. 1.Remote Monitoring 2.Easy to Install 3.Extensive Lineup
2:29