-
FORTELION 24V Battery Module Implementation Example: ugo, Inc. (For Service Robots)
The implementation of the FORTELION 24V battery module reduces maintenance and charging workload to improve work efficiency. In this video, we ask about what led to the implementation of the module at ugo, Inc. and the outcomes that result from the i
4:00
-
Differences between primary and secondary batteries
Batteries can be categorized by “Primary batteries,” which, like dry cell batteries, can only discharge electricity and “Secondary batteries,” which, like lithium-ion secondary batteries, not only discharge electricity but are also able to recharge.
1:22
-
Warning Regarding Lithium-ion Batteries
It has recently been confirmed that lithium-ion batteries manufactured and sold by Murata are being sold at some retailers and online shopping sites as individual batteries. (In some cases, they appear to be marketed specifically for use with "electr
7:07
-
High Drain Lithium Coin Batteries (CR) for IoT Devices
Excellent high-current discharge performance to support Low Power Wide Area (LPWA) data transmission.
2:45
-
Extended Temperature Lithium Coin Batteries (CR) for IoT Devices
Recommend for automotive & outdoor devices leveraging muRata’s heat resistant battery engineering design and utilization technologies.
2:57
-
Murata’s lithium-ion secondary batteries
Murata’s lithium-ion secondary batteries are adopted in a wide range of applications such as small electronic devices and electric tools, as well as home and industrial storage battery systems. We are developing new products optimal for electrificati
4:33
-
The introduction of the FORTELION 24V Battery Module
Murata has developed the FORTELION 24V Battery Module , which utilizes our unique FORTELION lithium-ion secondary battery and is the same size as a lead storage battery. Replacing your lead storage batteries with FORTELION 24V battery modules will re
6:21
-
The introduction of Olivine Type Lithium Iron Phosphate Lithium Ion Secondary Battery (FORTELION)
Murata’s "FORETELION" is a highly safe lithium ion secondary battery that uses olivine type lithium iron phosphate for its cathode with an expected life of over 15 years. Show more
4:21
-
Silver Oxide (SR) & Alkaline Manganese (LR) High Drain Batteries for Medical Devices
Murata offers SR Batteries&LR Batteries with excellent high-current discharge performance & high reliability to support medical device.
2:55
-
CT04120 Tutorial 3-(3) -Application example: Main power supply for small power equipment-
CT04120 can be used as a power supply formain power supply for small power equipment. This video shows the application examples of main power supply for small power equipment.
1:35
-
CT04120 Tutorial 3-(2) -Application example: Backup-
CT04120 can be used as a power supply for backup applications. This video shows the application examples of backup applications.
1:47
-
CT04120 Tutorial 3-(1) -Application example: Energy harvesting-
CT04120 can be used as a power supply for energy harvesting systems. This video shows the application examples of energy harvesting.
2:52
- Load More