Passionate Engineers Mastering the Art of Monozukuri
4:11
“What makes working at Murata so appealing?” From taking on the challenge of NHK’s “Makaizo no Yoru,” aired in February 2025, to the everyday trial and error on the development floor, Murata engineers share—in their own words—the excitement and fulfillment they have discovered through these hands-on experiences.
Related Videos
In All Videos
-
Play video Murata’s Vibration Sensor for High-Frequency Detection up to 20 kHz – Enabling Early Detection of Equipment Abnormalities –
Murata’s Vibration Sensor for High-Frequency Detection up to 20 kHz – Enabling Early Detection of Equipment Abnormalities –
Equipment often shows signs of failure—such as abnormal vibrations—before a sudden breakdown occurs. Murata’s vibration sensor detects high-frequency vibrations up to 20 kHz with a high signal-to-noise ratio, enabling early detection of abnormalities
2:44
-
Play video Introduction to Murata's Wi-Fi HaLow™ Modules (Type 2HK/2HL)
Introduction to Murata's Wi-Fi HaLow™ Modules (Type 2HK/2HL)
In this video, we take a look at the specifications and features of Murata's Wi-Fi HaLow™ modules (Type 2HK/Type 2HL). These products offer the high reliability required for industrial applications with a maximum output of +24 dBm (Type 2HK), enviro
2:26
-
Play video Murata RFIDs are blazing a new trail as they realize the future of next-generation smart inspections through embedded tire tags.
Murata RFIDs are blazing a new trail as they realize the future of next-generation smart inspections through embedded tire tags.
The work of inspecting tires places a burden on transport companies and dealers. With tires equipped with Murata's RFID tags, information such as the remaining tread depth can be centrally managed in the cloud by simply scanning the embedded tags. Th
1:35
-
Play video PTC Thermistor (POSISTOR) PRG series Application Example Resettable Fuses
PTC Thermistor (POSISTOR) PRG series Application Example Resettable Fuses
This video takes a look at an example of overcurrent protection using the PRG series of PTC thermistors as a resettable fuse. The PRG series has the following features:
3:52
-
Play video See How Humanoid Robotics Can Accelerate Real-World Automation
See How Humanoid Robotics Can Accelerate Real-World Automation
Humanoid robotics is moving from concept to real-world automation. But helping robots move, sense, connect and operate reliably requires more than AI.
2:04
-
Play video Waterproof Pressure Sensor in a Resin Package Demonstrations
Waterproof Pressure Sensor in a Resin Package Demonstrations
You can use this sensor in various applications, such as detecting falls, preventing false impact alarms, and tracking golf swing movements.
1:58