- 2x
- 1.75x
- 1.5x
- 1.25x
- 1x, selected
- 0.75x
- 0.5x
- Chapters
- descriptions off, selected
- captions settings, opens captions settings dialog
- captions off, selected
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Integrated Renewable Energy Control Solution efinnos Implementation Example
2:25
06 Dec. 2024
Must See: New Standard for Decarbonization and Cutting Electricity Bills! We look into the secrets of Kanazu Murata Manufacturing, which has been featured in many media outlets in Japan.
Related Videos
In Integrated Renewable Energy Control Solution efinnos
-
動画を再生 Wireless Sensor network solution for factories and buildings23 Jan. 2020
Wireless Sensor network solution for factories and buildings
Murata's Wireless Sensing Solution will enable you perform remote monitoring. Collected data can be used for the maintenance and efficiency improvement of factories and buildings. 1.Remote Monitoring 2.Easy to Install 3.Extensive Lineup
2:29
-
動画を再生 CT Sensor Unit05 Apr. 2021
CT Sensor Unit
Here is a wireless CT sensor unit that can be installed on equipment powered by a single-phase AC or three-phase AC power supply, such as three-phase heaters and motors that are essential to the infrastructure of buildings and factories, Show more..
2:06
-
動画を再生 Pulse Signal Unit05 Apr. 2021
Pulse Signal Unit
Here is a pulse signal unit that can be installed on existing sensors to automate data collection. The accumulated data can also be analyzed to determine the cause and the extent of the impact of any problems.
1:58
-
動画を再生 Temperature Humidity Sensor Unit05 Apr. 2021
Temperature Humidity Sensor Unit
Here is a wireless temperature and humidity sensor unit that can be easily installed and expanded. Show more...
2:55
-
動画を再生 Vibration Sensor Unit05 Apr. 2021
Vibration Sensor Unit
Here is a wireless vibration sensor unit that achieves a wide range of measurement frequencies and long battery life for its vibration sensor unit by making use of the company’s knowledge of piezo-ceramic elements that was cultivated over Show more..
2:33
-
動画を再生 Wi-Fi® sensing for child presence detection Overview02 Apr. 2021
Wi-Fi® sensing for child presence detection Overview
The Wi-Fi® sensing solution features 1: easy installation, 2: flexibility of installation location, and 3: a wide detection area, contributing to the new standard for NCAP compliance.
1:23